Question of NVT4857UK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question of NVT4857UK

846 Views
wujie08
Contributor I

#Question of NVT4857UK# TomasVaverka

I plan to use NVT4857UK chip in my project to convert voltage SD card IO signal provided by FPGA from 1.8v to 3.3v. I have few questions from the spec of NVT4857UK:

1. For the pin VCCB, is it an output signal of this chip? or an input signal need from host?  and does VCCB equal to VLDO? 

2. For the resistor R1,R2 on the pic of page 4, do these resistor have already been integrated in this chip or need to be added on PCB?

3. For the resistors R3, R4, R5 need to be added on PCB, am I right?

thanks a lot.

Tags (1)
0 Kudos
2 Replies

761 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Wu,

1. VCCB is VLDO output pin and requires an external capacitor between this pin and ground for proper operation of the LDO. Its typical value is 2.2 uF.

2&3. All resistors shown in the functional diagram are internal.

Best regards,

Tomas 

0 Kudos

761 Views
wujie08
Contributor I

thanks a lot, Tomas 

0 Kudos