Question about Fault collection and control unit(FCCU) for Automotive Devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about Fault collection and control unit(FCCU) for Automotive Devices

1,527 Views
inhojeon
Contributor III

Hi, All.

I'll design to ADAS like a below image schematics.

I research parts : CAN CPU & PMIC for CPU ; like below condition.

  - PMIC for CPU

  1. Automotive Spec.

  2. Monitoring total powers & Using functional safety blocs ASIL(Automotive Safety Integrity Level) type PMIC.

  3. Watch-dog 

  4. FCCU(Fault collection and control unit)

  - CAN CPU

1. CAN Controller 

2. Watch-dog

Best Regards,

Inho Jeon.

pastedImage_1.png

3 Replies

1,242 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Inho,

As for the PMIC, I would recommend our FS65xx SBC family that meets all your specified requirements (AEC-Q100
Grade 0 automotive qualification, configurable fail-safe/fail silent safety behavior and features, windowed watchdog, safety inputs for FCCU monitoring).

pastedImage_1.png

Regarding the CAN MCU, I suggest either the MagniV S12 ZVC (16-bit) or S32K (32-bit) family of AEC-Q100 qualified MCUs.

Best regards,

Tomas

1,242 Views
inhojeon
Contributor III

Hi Tomas,

I have a additional question.

If it is not bulit-in FCCU fuctions of CPU(ADAS CPU), is it possible use FCCU?

Because, ADAS CPU & PMIC for ADAS CPU is not built-in FCCU fuctions.

Best regards,

Inho Jeon.

0 Kudos

1,242 Views
inhojeon
Contributor III

Hi Tomas,

Thank you for your reply.

I have a question.

Is the parts you suggested working only AUTOSAR OS? Or is possible linux like low cost OS?

I prefer low cost OS like linux.

Best regards

Inho Jeon

0 Kudos