Problems with remapping of CCSR (MPC8548)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with remapping of CCSR (MPC8548)

1,792 Views
Timmo
Contributor I
Hello.
I'm trying to programm a bootloader for the MPC8548 but I have big problems with the MMU and remapping of the CCSR. After Reset the CCSR is located at 0xFF70_0000. So at first I init the TLB1 Entry 1 with the following:

    lis     %r6,FSL_BOOKE_MAS0(1, 1, 0)@h
    ori     %r6,%r6,FSL_BOOKE_MAS0(1, 1, 0)@l

    lis     %r7,FSL_BOOKE_MAS1(1, 1, 0, 0, BOOKE_PAGESZ_1M)@h
    ori     %r7,%r7,FSL_BOOKE_MAS1(1, 1, 0, 0, BOOKE_PAGESZ_1M)@l
   
    lis     %r8,FSL_BOOKE_MAS2(0xFF700000, MAS2_I)@h
    ori     %r8,%r8,FSL_BOOKE_MAS2(
0xFF700000, MAS2_I)@l

    lis     %r9,FSL_BOOKE_MAS3(
0xFF700000, 0, (MAS3_SX|MAS3_SW|MAS3_SR))@h
    ori     %r9,%r9,FSL_BOOKE_MAS3(
0xFF700000,0,(MAS3_SX|MAS3_SW|MAS3_SR))@l

    mtspr   MAS0,%r6
    mtspr   MAS1,%r7
    mtspr   MAS2,%r8
    mtspr   MAS3,%r9
    isync
    sync
    .long 0x7C0007A4    //tlbwe, compiler doesn't support this opcode


After that I can set some GPIOs so I can see that it works. Now I wanted to relocate the CCSR to 0xE000_0000. So I followed the Instructions of the Manual Page 4-4:

    lis        %r3,0xFF700000@h
    ori        %r3, %r3,
0xFF700000@l
   
    lwz        %r4,0(%r3)                    /* Read CCSRBAR */
    isync
    lis        %r4,(0xE0000000 >> 12)@h        /* New Address for CCSRBAR */
    ori        %r4, %r4, (
0xE0000000 >> 12)@l
    stw        %r4, 0(%r3)
    li         %r3, 0xFFFFF000@h             /* Read somewhere in ROM */
    ori        %r3, %r3, 0xFFFFF000@l
    lwz        %r4, 0(%r3)
    isync


    /* Update TLB1,1 for new Address */
    lis     %r6,FSL_BOOKE_MAS0(1, 1, 0)@h
    ori     %r6,%r6,FSL_BOOKE_MAS0(1, 1, 0)@l

    lis     %r7,FSL_BOOKE_MAS1(1, 1, 0, 0, BOOKE_PAGESZ_1M)@h
    ori     %r7,%r7,FSL_BOOKE_MAS1(1, 1, 0, 0, BOOKE_PAGESZ_1M)@l
   
    lis     %r8,FSL_BOOKE_MAS2(
0xE0000000 , MAS2_I)@h
    ori     %r8,%r8,FSL_BOOKE_MAS2(
0xE0000000 , MAS2_I)@l

    lis     %r9,FSL_BOOKE_MAS3(
0xE0000000,0,(MAS3_SX|MAS3_SW|MAS3_SR))@h
    ori     %r9,%r9,FSL_BOOKE_MAS3(
0xE0000000,0,MAS3_SX|MAS3_SW|MAS3_SR))@l

    mtspr   MAS0,%r6
    mtspr   MAS1,%r7
    mtspr   MAS2,%r8
    mtspr   MAS3,%r9
    isync
    sync
    .long 0x7C0007A4    //tlbwe


    /* Read the content of CCSRBAR from new Address */
    lis        %r3,
0xE0000000@h
    ori        %r3, %r3,
0xE0000000@l
    lwz        %r4,0(%r3)


After that I don't have any access to the CCSR. What am I doing wrong?

Advice:
FSL_BOOKE_MASX-Macros are from uboot 1.3.4:
#define FSL_BOOKE_MAS0(tlbsel,esel,nv) \
        (MAS0_TLBSEL(tlbsel) | MAS0_ESEL(esel) | MAS0_NV(nv))
#define FSL_BOOKE_MAS1(v,iprot,tid,ts,tsize) \
        ((((v) << 31) & MAS1_VALID)             |\
        (((iprot) << 30) & MAS1_IPROT)          |\
        (MAS1_TID(tid))                |\
        (((ts) << 12) & MAS1_TS)                |\
        (MAS1_TSIZE(tsize)))
#define FSL_BOOKE_MAS2(epn, wimge) \
        (((epn) & MAS3_RPN) | (wimge))
#define FSL_BOOKE_MAS3(rpn, user, perms) \
        (((rpn) & MAS3_RPN) | (user) | (perms))

I hope somebody can help me


Message Edited by Timmo on 2008-10-21 11:13 AM
0 Kudos
Reply
2 Replies

631 Views
genuap
NXP Employee
NXP Employee
You need an isync after the tlbwe instructions. I see that you have them prior to them. An msync (or sync) would be sufficient prior to them, when writing the mtspr's. But you need an isync right after, since there's no guarantee how long the tlbwe is going to take to execute.

 ... Paul

0 Kudos
Reply

631 Views
Timmo
Contributor I
Hello.
I added an isync after each tlbwe but the problem is still the same.
Any other idea? The Freescale support can't help me either until now.
0 Kudos
Reply