Problems with NVM in MC1322x after reset.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with NVM in MC1322x after reset.

4,807 Views
ccruces
Contributor I

I am working with a OnOffSwitch application (with Non Volatile Memory and with router role)that I get direcltly from the Beekit using Beestack Codebase 3.0.1. I load it in a MC1322x Sensor Node. I have not made any modications in the code get from the beekit, however it doesn´t work properly after I make a reset.

When I switch on the MC1322x Sensor Node for the first time after loading the code, it associates correctly with the coordinator, however after making a reset, the device has the led 1 blinking, and although I press the button 1 it remains blinking, it doesn´t make anything and it is imposible to rejoin with the coordinator. What is happening?
With a SARD board and codebase 2.0.0, it works properly, why not with MC1322x Sensor Node and codebase 3.0.1
?

0 Kudos
Reply
12 Replies

1,517 Views
admin
Specialist II

I am also interested in other codebase versions for the ZigBee, MAC and SMAC codebases.

 

The last few days I had tested the beacon functionality with the MAC codebase. To start

a non-beaconed network isn't a problem. The MAC codebase contains a example project to start and run a non-beaconed network. But for a beacon netwok there is no example project.

 

When I follow the instructcions to start a beacon network in the 802.15.4 MAC MyWirelessApp User's Guide and the 802.15.4 -2003 specifications The beacon network doens't work correctly. Have someone of you experience with a beacon network for the Freescale mc13224 platforms?

 

 

 

 

 

0 Kudos
Reply

1,517 Views
MichaelV
Senior Contributor II

In response to: Jan2 regarding beacon enabled PAN using ARM7 MAC codebase 2.0.0

 

Same here. Have you had any luck in solving this? I'm getting heaps of SYNC_LOSS indications with reason PAN Conflict (but there's only one coordinator and one device in my system).

0 Kudos
Reply

1,517 Views
tpicon
Contributor II

sorry michael, i didn't solve this

if you wish send me a private e-mail  tpicon@scenario.ind.br

 

Regards

0 Kudos
Reply

1,517 Views
mack23
Contributor I

Has anyone created a working network with beaconing on MC13224 platform? According to documentation, there is no way to do that using freescale's MAC library

0 Kudos
Reply

1,517 Views
Elisa
Contributor III

On the Freescale website there is finally the codebase 3.0.2 for MC1322x v 2.0

 

This this the last codebase useful for this chip version and should solve some problem of previous codebase version.

 

http://www.freescale.com/webapp/search/Serp.jsp?QueryText=beekit&fsrch=1&isAdvanceSearch=false&showC...


0 Kudos
Reply

1,517 Views
Elisa
Contributor III

Hi, I created a group about MC1322x and ZigBee. If you want, you can I join it.

 

http://groups.google.it/group/freescale-mc1322x-and-zigbee

0 Kudos
Reply

1,517 Views
Elisa
Contributor III
Hi, I'm working with with codebase 3.0.1 and I have more or less the same problem: I want' my MC1322x Low Power Node goes to sleep and sends a test message to coordinator when it wake up. But sometimes, after wake up it loses its parents and like in you case "the led 1 blinking, and although I press the button 1 it remains blinking, it doesn´t make anything and it is imposible to rejoin with the coordinator. What is happening?"
0 Kudos
Reply

1,517 Views
tpicon
Contributor II

Hi Elisa

Nowadays i'm working with codebase 3.0.3 but the problem still happens. If you wish we can talk about via e-mail

My e-mail is  tpicon@scenario.ind.br

Regards.... 

 

 

0 Kudos
Reply

1,516 Views
ccruces
Contributor I

Freescale support has told me that it appears that codebase 3.0.1 for ARM7 has an error. If the MC1324 Silicon version of your chip is 2.0 you should upgrade from 3.0.1 to 3.0.2. If the version is 2.1 you should upgrate to 3.0.3 (From silicon rev 2.0 to rev 2.1 ROM changes were made, and then the drivers have changed for new rev 2.1)

 

My Silicon rev is 2.0, but I don´t have the codebase 3.0.2 because it isn´t avalaible in the web. So I have not checked this solution. I am waiting a reply from freescale support to get the codebase 3.0.2

 

tpicon, which is the silicon rev of your chip? (you may see it in the printed part number of the chip)

0 Kudos
Reply

1,517 Views
Elisa
Contributor III

On the Freescale website there is finally the codebase 3.0.2 for MC1322x v 2.0

 

This this the last codebase useful for this chip version and should solve some problem of previous codebase version.

 

http://www.freescale.com/webapp/search/Serp.jsp?QueryText=beekit&fsrch=1&isAdvanceSearch=false&showC...

0 Kudos
Reply

1,517 Views
tpicon
Contributor II

In my kits i have the silicon revision 2.0

I understood the problem now...i didn't know about the codebase 3.0.2. Thanks

 

Anyway, i think that we can change ideas (talk about) about ZigBee because i don't know anyone more that works with this platform in my town or state...

 

If you wish my e-mail is  tpicon@scenario.ind.br

 

 

Regards

 

0 Kudos
Reply

1,517 Views
tpicon
Contributor II

I have the same problem...

At the moment i can't solve this but i'm trying...

 

This forum is very calm...If you wish we can change ideas...

My e-mail is   tpicon@scenario.ind.br

 

Regards

Tiago 

0 Kudos
Reply