Problem in using MPC8260 in 'Configuration Master' (multiplocessor mode)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in using MPC8260 in 'Configuration Master' (multiplocessor mode)

1,745 Views
h_humble2001
Contributor I
Hi,
I am using MPC8260 in Configuration Master in 2 boards. At power-up MPC executes from flash but crashes after about (0.5 sec). It is also observed that if the board is powered-up for a few minutes then the MPC works fine. It seemed that when the system is heated a little bit it works fine. I have two identical boards. One of them is working perfectly fine and the other one is not.
 
Please I need suggestions and possible reasons of this behaviour.
 
Thanks in advance.
 
John
0 Kudos
Reply
1 Reply

1,036 Views
genuap
NXP Employee
NXP Employee
Do you know if it fetched the reset word? (Is RSTCFG pulled low? - to be a config master). You could try to pull RSTCONF high temporarilarly to use a 'default' setting to see if it's not getting the config word correctly.

Do you have a scope or analyzer on there to see how many bus accesses went on before it died?

Also, check your pullups on POR, HRESET & SRESET. They should be in the 2k range.


0 Kudos
Reply