Hi,
this is the first time I'm posting here, so ready to improve if needed.
Currently I'm working with the sja1105 ethernet board and I'm trying to learn how to use it from the User software manual and through the "sja1105smbevm_tc10example" which I attached here.
I continue to experience a problem during debugging inside a vTaskDelay(), in particular:
here's the tasks priority
It hang after entering this vTaskDelay() inside can_task()
The console shows
Trying to debug more closely at that point I think the problem is around here:
Looking at wireshark view it also stops the capture at that point!!
Once I power recycle the board and unplug the debugger wireshark starts to capture again:
Pls help, thank you a lot
Hi @Bongio98 ,
I understand your issue. Can you tell me to which position the rotary encoder on the SJA1105SMBEVM is set to?
Additionally, I'd like you to try to set it to position 4 and try again. Do you still see this issue?
Thank you.
Best regards
Kevin