Port u-boot to MPC8360 / MPC8358

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port u-boot to MPC8360 / MPC8358

2,601 Views
Elison
Contributor I
Dear All,

My task is to port linux to MPC8358E on a custom board. Before that I need to port u-boot to the same.

I did not find any information in all the documentation/forums I have searched so far. (If there is one, I am extemely sorry to have missed it)

The MPC8358 is connected with a FLASH on the local bus and  DDR2 RAM. A 32 KB I2C EEPROM is provided for the first boot.

I understand that I need to set to reset source pins the first time so as to load the reset configuration words from the I2C EEPROM.

The I2C EEPROM will have data in the format as specified in the datasheet.

From what I understand, I need to have some code running that initializes the UART (?) and copies the received data to some RAM (?) location. Then I need to build and transfer the u-boot binary to the MPC and give the control to u-boot. I am (kind of) clear with what to do next once u-boot is running, but how do I port u-boot to the board?

I have a very general idea and do not know from where to actually get started. Can anyone please throw some light on this?


Best Regards,

Elison
0 Kudos
Reply
1 Reply

615 Views
sachinr
Contributor I
Ellison,

All the code for u-boot & Linux kernel port to 8358/8360 is already available at the Freescale website:
freescale.com/powerbsp

--

Sachin
0 Kudos
Reply