Pls help check the different with TJA1055T/3/1J and TJA1055T/3/1.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pls help check the different with TJA1055T/3/1J and TJA1055T/3/1.

316件の閲覧回数
Leyla
Contributor I

Dear Team,

 

Pls help check the different with TJA1055T/3/1J and TJA1055T/3/1.

What means the end of "J"?

 

Thanks.

0 件の賞賛
1 返信

306件の閲覧回数
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Leyla,

TJA1055T/3/1 - This is the type name for the dual sourced version of the 3V (VIO) version. It can be supplied from either the SSMC wafer fab or from the ICN8 wafer fab.TJA1055T/3/1J - This is the full orderable part number of the TJA1055T/3/1, the -J indicates that this is the tape and reel packing method.

Best regards

Pavla

0 件の賞賛