Pls help check the different with TJA1055T/3/1J and TJA1055T/3/1.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pls help check the different with TJA1055T/3/1J and TJA1055T/3/1.

310 Views
Leyla
Contributor I

Dear Team,

 

Pls help check the different with TJA1055T/3/1J and TJA1055T/3/1.

What means the end of "J"?

 

Thanks.

0 Kudos
1 Reply

300 Views
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Leyla,

TJA1055T/3/1 - This is the type name for the dual sourced version of the 3V (VIO) version. It can be supplied from either the SSMC wafer fab or from the ICN8 wafer fab.TJA1055T/3/1J - This is the full orderable part number of the TJA1055T/3/1, the -J indicates that this is the tape and reel packing method.

Best regards

Pavla

0 Kudos