Package markings for PCF8582C2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Package markings for PCF8582C2

1,968 Views
mgreenhalgh
Contributor II

I need to know the meaning of the package markings for the PCF 8582C2T03,112.

The markings are as follows:

Device 1:

8582C-2

M1 01

nG026

Device 2:

8582C-2

67 02 (Possible G7 02)

n6107 (possible nG107)

6Computrol_8582 date req3.bmp

3 Replies

1,245 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mark,

First off, the PCF8582C-2T/03 is a discontinued part type.

 

The top line is an abbreviated part type due to marking limitation of 7 characters for this package outline.

On the second line the M1 01 and G7 02 are diffusion batch ids.

The last line of marking is n=Bangkok, Thailand assembly site followed with a "G" (not a 6) for the RoHS Lead-Free status. Then the  026 and 107 are date codes.

 

Hope it helps.

 

Best regards,

Tomas

0 Kudos

1,245 Views
mgreenhalgh
Contributor II

Thanks for the response.  Do you happen to know the date code format?  Y/WW, YY/M, etc?

0 Kudos

1,245 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mark,

Apologies for my late response. 

The date code format is Y/WW:

026 = 2010/ww26 

107 = 2011/ww07 

Best regards,

Tomas