PTN5150A DFP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN5150A DFP mode

888 Views
gady
Contributor I

Hi,

i want to know the application note for DFP mode, i have some issue with this mode.

1. i connect pin 4 (vbus_det) to vbus of the connector and PTN5150A don't recognized any connection ( i plug camera in my cards)

2. now pin 4 (vbus_det) are floating and PTN5150A do recognize the camera.

i add the schematic here.

the connector get vbus (5v) after PTN5150A recognize detection of USB all work when pin 4 are floating.(i remove R111). but in this case i have another issue and that's the camera is recognize on USB3.0 only in one direction of connection and in other direction it's recognize on USB2.1.

 

thank you,

 

Tags (1)
0 Kudos
Reply
4 Replies

867 Views
gady
Contributor I

1. In DFP mode , when PTN5150A recognize USBi use ADR/CON_DET to give vbus to the connector USB and to VBUS_DET pin

2. The PORT pin is connected to VDD in the schematic it's 5V

3. i fix the mistake , now the pin it's floating then it will be a output 

steel , if i set the VBUS_DET pin floating the PTN5150A recognize the connection of camera , but if i set VBUS_DET to VDD it doesn't recognized so it's right or no? (the camera don't give VBUS i need to produce him VBUS)

thank you.

0 Kudos
Reply

855 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:Directly connect VBUS_DET pin with your type C receptacle VBUS to try.

0 Kudos
Reply

848 Views
gady
Contributor I

i do it the first time the PTN5150A don't recognized any connection

0 Kudos
Reply

876 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:How is the connection way between VBUS_DET pin and USB_CON_VBUS?

I didn’t see they are connect with together.

2: In the standalone mode with DFP configuration the PORT pin should be connected to VDD.

3:You can’t pull up ID/ADR to VBUS, please see below limiting values

guoweisun_0-1702434836114.png

 

0 Kudos
Reply