PTN36241 C1/C2 pins issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN36241 C1/C2 pins issues

219 Views
Johnnie
Contributor I

Hello NXP expert,

Host (PC) side can't connect by USB3.0 calble with device when redriver C1/C2 are "open" status.

But connection are working if we have "high level" of them(C1/C2). May I know why have disconnection issues under C1/C2 are open status?

Thanks 

 

0 Kudos
3 Replies

152 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you mean the C1/C2 of PTN36241?

0 Kudos

138 Views
Johnnie
Contributor I

Yap.  C1/C2 Pin12 & Pin 6

0 Kudos

194 Views
Johnnie
Contributor I
  • Default: w/ redriver and C1 = C2 = Open -> no Tx/Rx signaling.
  • DOE1: w/ redriver and C1 = C2 = Hi -> eye diagram pass, but time-shifted
  • DOE2: w/o redriver and short Tx/Rx directly-> eye diagram pass
0 Kudos