PTN36043 USB 3.1 MUX / RETIMER - Is it OK to swap the plus and minus pins on the input and output to facilitate routing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN36043 USB 3.1 MUX / RETIMER - Is it OK to swap the plus and minus pins on the input and output to facilitate routing?

733 Views
donaldruss
Contributor II

#PTN36043 USB 3.1 MUX / RETIMER  - Is it OK to swap the plus and minus pins on the input and output to facilitate routing as with simple MUX ICs or does the Retimer require the polarity to be correct?  Better to have VIAs on one pair than 5.

pastedImage_2.png

Thanks in advance.

Don

i.MX8M USB OTG super speed support‌ 

Tags (1)
0 Kudos
1 Reply

691 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Don,

Yes, you can swap the +/- on both the input side (AP side) and connector sides (both CON1 and CON2). 

Best regards,

Tomas

0 Kudos