PTN3365 HDMI level shifter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PTN3365 HDMI level shifter

13,414件の閲覧回数
shichinhuang
Contributor I

Hi,

Could anybody from NXP help me to comment if I can use PTN3365 (NXP HDMI level shifter)

design in the circuit as attachment.

タグ(1)
0 件の賞賛
返信
5 返答(返信)

13,229件の閲覧回数
shichinhuang
Contributor I

Hi Jose,

Thank you for your answer.

Yes, the 3.1V is HDMI DC level.

Before the PTN3365, the circuit has AC couple capacitors, so it will block DC level and become 0V. But the PTN3365 should change DC level of HDMI signal from 0V to 3.1V(HDMI DC level),is it correct? See below picture for more detail.

Thanks!

pastedImage_1.png

pastedImage_2.png

Sincerely,

Shichin

0 件の賞賛
返信

13,229件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Shichin,

Thanks for the clarification, now I understand your question.

The answer is Yes, you can use the PTN3365 to change back the DC level of HDMI signal from 0V to 3.1V (HDMI DC level) after the AC couple capacitor.

Thanks,

Jose

13,229件の閲覧回数
shichinhuang
Contributor I

Hi Jose,

Okay.

Thank you for your help!

Sincerely,

Shichin

0 件の賞賛
返信

13,229件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately no, PTN3365 cannot modify the offset the of the signal, PTN3365 can only be used as  a level shifter device to convert the voltage level of the HDMI signals.

Regards,

Jose

NXP Semiconductor

0 件の賞賛
返信

13,229件の閲覧回数
shichinhuang
Contributor I

Hi Jose,

Thank you for your answer.

Yes, the 3.1V is HDMI DC level.

Before the PTN3365, the circuit has AC couple capacitors, so it will block DC level and become 0V. But the PTN3365 should change DC level of HDMI signal from 0V to 3.1V(HDMI DC level),is it correct? See below pictures for more detail.

Thanks!

pastedImage_1.png

pastedImage_2.png

Sincerely,

Shichin

0 件の賞賛
返信