Hi,
We have a ls1028 customer board, build the system by OpenIL V1.10 ,used the configs nxp_ls1028ardb-64b_defconfig.On display, we used PTN3356R1 to convert DisplayPort to VGA. The schematic is refer to the application note(AN11590).
When powered up, the screen show nothing, but according to the booting log we find the DP driver is alread readed the EDID infomations from the screen.
[ 4.836757] [drm] Initialized mali-dp 1.0.0 20160106 for f080000.display on minor 0
[ 4.836774] drivers/gpu/drm/bridge/cadence/cdns-dp-core.c: cdns_dp_connector_detect
[ 4.838083] drivers/gpu/drm/bridge/cadence/cdns-dp-core.c: cdns_dp_connector_get_modes
[ 4.878837] cdns-mhdp-imx f200000.display: 0,ff,ff,ff,ff,ff,ff,0
[ 4.878845] cdns-mhdp-imx f200000.display: mfg_id:30,ae
[ 4.878848] cdns-mhdp-imx f200000.display: prod_code:bf,60
...
3 questions want to confirm:
1) should I config the registers of the PTN3356? Does it work if the peripheral circuit is okay?
2)Does the linux dts need to be modified? PTN3356 just use DP_LANE0 and DP_LANE1, but the default setting of ls1028ardb is using DP_LANE0~DP_LANE3. the DP lane setting in dts is:
lane-mapping = <0x4e>;
3)Are there any other settings for DP parameters or LCD controller?
Thanks.