PPS signal on LS1021A TSN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PPS signal on LS1021A TSN

Jump to solution
1,069 Views
muaslam
Contributor I

Hi,
Currently, I am using LS1021A TSN for clock synchronization. I wonder if the switch has exposed PPS port to measure clock synchronization? If yes, may I learn how to configure it?
I could not find much information about it in user manual.
https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-10.pdf

Tags (3)
0 Kudos
Reply
1 Solution
1,051 Views
bpe
NXP Employee
NXP Employee

LS1021A-TSN does not have provisions for PPS output. SJA1105T cannot generate
them, on LS1021A these signals are multilexed and their corresponding pins are
used for other purposes. If your application requires both L2 TSN switch and PPS
outputs, consider using the next generation TSN board, LS1028A-RDB

 

Best Regards,
Platon

View solution in original post

0 Kudos
Reply
1 Reply
1,052 Views
bpe
NXP Employee
NXP Employee

LS1021A-TSN does not have provisions for PPS output. SJA1105T cannot generate
them, on LS1021A these signals are multilexed and their corresponding pins are
used for other purposes. If your application requires both L2 TSN switch and PPS
outputs, consider using the next generation TSN board, LS1028A-RDB

 

Best Regards,
Platon

0 Kudos
Reply