PPS signal on LS1021A TSN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PPS signal on LS1021A TSN

ソリューションへジャンプ
1,067件の閲覧回数
muaslam
Contributor I

Hi,
Currently, I am using LS1021A TSN for clock synchronization. I wonder if the switch has exposed PPS port to measure clock synchronization? If yes, may I learn how to configure it?
I could not find much information about it in user manual.
https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-10.pdf

タグ(3)
0 件の賞賛
返信
1 解決策
1,049件の閲覧回数
bpe
NXP Employee
NXP Employee

LS1021A-TSN does not have provisions for PPS output. SJA1105T cannot generate
them, on LS1021A these signals are multilexed and their corresponding pins are
used for other purposes. If your application requires both L2 TSN switch and PPS
outputs, consider using the next generation TSN board, LS1028A-RDB

 

Best Regards,
Platon

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,050件の閲覧回数
bpe
NXP Employee
NXP Employee

LS1021A-TSN does not have provisions for PPS output. SJA1105T cannot generate
them, on LS1021A these signals are multilexed and their corresponding pins are
used for other purposes. If your application requires both L2 TSN switch and PPS
outputs, consider using the next generation TSN board, LS1028A-RDB

 

Best Regards,
Platon

0 件の賞賛
返信