PN7462 dual smartcard interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 dual smartcard interface

639件の閲覧回数
kralsemo06
Contributor I

Hi,

I have a contact and contactless smart card reader project. I'm thiking of using the PN7462 series for the project.PN7462 supports a slot contact smart card reader. I see in the datasheet that it can increase the number of contact smart card slots. Can we confirm this ? Can u provide detailed technical support(e.g. schematic design)

 

Best regards,

0 件の賞賛
1 返信

626件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the design as the PN7462 family HW user manual for it.

URL:https://www.nxp.com/docs/en/user-guide/UM10858.pdf

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛