Hi,
I have a contact and contactless smart card reader project. I can't use PN7462 to stock status.
I want support ISO 7816 protocol externally.
I Think PN7362 7.pin is ok for this case ( ATX_B SPI slave data input (MOSI_S)/I2C-bus serial data I/O (SDA_S)/HSUART TX)
Do you think this is possible. I'm waiting for your help. Thanks.
Best regards,
Solved! Go to Solution.
Hello,
Yes, It is OK for the application .Please use the pins as the below:
Hope it help you.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hello,
Yes, It is OK for the application .Please use the pins as the below:
Hope it help you.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------