PN7362 external ISO 7816 support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7362 external ISO 7816 support

Jump to solution
774 Views
kralsemo06
Contributor I

Hi,

I have a contact and contactless smart card reader project. I can't use PN7462 to stock status. 

I want support ISO 7816 protocol  externally.

I  Think  PN7362 7.pin is ok for this case  ( ATX_B SPI slave data input (MOSI_S)/I2C-bus serial data I/O (SDA_S)/HSUART TX) 

Do you think this is possible. I'm waiting for your help. Thanks.

Best regards,

0 Kudos
1 Solution
746 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, It is OK for the application .Please use the pins as the below:

fangfang_1-1633924448134.png

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

 

View solution in original post

0 Kudos
1 Reply
747 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, It is OK for the application .Please use the pins as the below:

fangfang_1-1633924448134.png

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

 

0 Kudos