Good Morning.
We are doing a little design to detect TAG based on Arduino.
I think I have correctly copied the protoboard design, but I have tested and arduino does not detect the PN7150 by I2C.
I have doubts with the PVDD output. Does it have to be connected with VBAT ?, or is PVDD only used to select the I2C port with a resistor in I2CARDx? I have doubts about the connection that appears in the PIN: VBAT and PVDD in parallel
In I2C is a pull-up resistor necessary? I don't see it in the protoboard design.
Attached your schematic, and the schema that I am using.
Thank you so much for everything.
Hello
At the moment compared our PCB, with your reference OM5578 / PN71505:
R2 is required
PVDD and VBAT need to be connected to 3.3V
only VBAT1 to 5V is not enough
With this connection our PCB seems to start working. I still haven't gotten it to communicate over I2C, but it's progress
Thank you so much for everything
Hello,
You are welcome.
Thanks for your updated information.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hello,
Your schematic seems there is no question. Please check if has the pull-up in software due to there is not pull-up in schematic.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------