PN5180 TEST ANALOG MODE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 TEST ANALOG MODE

485 Views
rboporto
Contributor I

Hello, 

I want to use AUX1 as analog output for debugging. 

In "Table 50: ANALOG TEST SIGNALS" from datasheet: 

"DAC_VALUE_OUT 0h Analog output of value defined in register DAC_VALUE"

 

The problem is that I can't found the DAC_VALUE register. 

The nearest thing that I've found is EEPROM fields TbDac1 (0xf8) TbDac2 (0xf9) but I'm not sure how exactly control the DAC in AUX1. 

 

Tags (2)
0 Kudos
1 Reply

475 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 NFC Cockpit can  confige  it. Please find the more information as the link.

URL:https://www.nxp.com/docs/en/application-note/AN11744.pdf.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos