PN5180 EMV & ISO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 EMV & ISO

269 Views
HoYeongJang
Contributor I

Hello,

 

I want to know Is it PN5180 satisfactory with EMV and ISO at the same time?

As I know EMV has to satisfy distance 4cm.

However, ISO has to satisfying distance more than 5cm.

 

How can I satisfying two conition?

Just using PN5180, Can I do this? Or I have to more something to this?

 

Please let me know details.

Thanks.

0 Kudos
1 Reply

237 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @HoYeongJang 

Sure, of course you can. First, the PN5180 is working on ISO/IEC 14443 before it is EMVCO compliant.
First of all, you have PN5180 working following the ISO/IEC14443 protocol standard.
Secondly, the EMVCO feature is implemented under the above conditions.
You can refer to SW352236, which contains routines on how to implement EMVCO.

BR

kelly

0 Kudos