I have connected LS1088ARDB_PB PCIe bus interface connected with Tp-Link 10Gbps Ethernet adaptor (Model No: TX401) card.
I could able to load the Kernel Object file, but immediately it is throwing PCI Bus Error. Here is the Error
[ 2262.949050] pcieport 0001:00:00.0: AER: PCIe Bus Error: severity=Corrected, type=Data Link Layer, (Transmitter ID)
[ 2262.949053] Internal error: synchronous external abort: 96000210 [#1] PREEMPT SMP
[ 2262.949055] Modules linked in: atlantic(O+)
[ 2262.959422] pcieport 0001:00:00.0: AER: device [1957:80c0] error status/mask=00001000/00006000
My question here is, will LS1088ARDB_PB will support the 10Gbps Ethernet card?
Please help me.
Thanks & Regards
Suresh