PCF8563 add 1 or 2 external capacitor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8563 add 1 or 2 external capacitor?

Jump to solution
1,558 Views
qpgydlh
Contributor I

Hi,

I‘m not sure should I add 1 capacitor on OSCI or 2 capacitor on OSCI ,OSCO pin? Is it 8pF too small?

The crystal CL is 12.5pF.And the crystal is nearly close to the PCF8563 pin.

As the Datasheet tips show Cload= [ (Ctrim*Cosco)/(Ctrim+Cosco) ]  should I add 1 external capacitor 22pF on OSCI pin just fine ? OSCO pin no need external capacitor because OSCO has already have internal capacitor?

thanks!

16486055343591.png

 

{129BC8F6-38A5-486A-92AF-51901A640E78}.png 16486051748284.png

Tags (1)
0 Kudos
1 Solution
1,548 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please refer to below picture mentioned value:

guoweisun_0-1648607665352.png

 

View solution in original post

0 Kudos
6 Replies
1,506 Views
guoweisun
NXP TechSupport
NXP TechSupport

No exactly value but around 600mV.

0 Kudos
1,549 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please refer to below picture mentioned value:

guoweisun_0-1648607665352.png

 

0 Kudos
1,456 Views
qpgydlh
Contributor I

What are the requirements for the driver level of crystal ?

Is it continuous  drive the crystal?or just in start-up?

0 Kudos
1,454 Views
guoweisun
NXP TechSupport
NXP TechSupport

 It is the continuous  drive  internal  of IC.

0 Kudos
1,516 Views
qpgydlh
Contributor I

Another question,What is the operation voltage range in OSCI (Oscillation amplitude)and OSCO pin?not absolute maximum range. 

0 Kudos
1,505 Views
guoweisun
NXP TechSupport
NXP TechSupport

No exactly value but around 600mV.

0 Kudos