PCF2131TF Vbat > Vdd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF2131TF Vbat > Vdd

Jump to solution
520 Views
jasonwilliams_a
Contributor I

Hello,

In our application we have a supercap connected to Vbat on the PCF2131TF. Our logic is running at 3.3V but we also have a 5V rail available. The PCF2131TF is running in I2C mode.

We would like to connect the supercap to charge from the 5V rail for a longer RTC running time when system power is removed.

Will the PCF2131TF support having the Vbat rail at 5V while Vdd is 3.3V?

Tags (2)
0 Kudos
1 Solution
464 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jason.

Yes, the PCF2131TF will operate with those voltages at Vbat and Vdd.  

BR, Tomas

View solution in original post

1 Reply
465 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jason.

Yes, the PCF2131TF will operate with those voltages at Vbat and Vdd.  

BR, Tomas