Hello kaifalkenberg,
Thank you for using the NXP community.
Have you considered using the Aging_offset register to correct the crystal aging effects?
The accuracy of the frequency of a quartz crystal depends on its aging. The aging offset adds an adjustment, positive or negative, in the temperature compensation circuit which allows correcting the aging effect.
The aging offset bits allow a frequency correction of typically 2 ppm per AO[3:0] value, from -14 ppm to +16 ppm.
Please review the chapter 7.4 from datasheet for further information.
Regards,
David