PCB Layout for MW7IC915N

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCB Layout for MW7IC915N

829 Views
chris_zhang
Contributor II

Hi,

The reference design of MW7IC915N is 2-layer PCB, and we want to change the PCB to 6-layer, but we has no idea if this solution is available? if yes, please advise if there are any design issue to improve? thanks.

Labels (1)
  • RF

Tags (2)
0 Kudos
2 Replies

798 Views
chris_zhang
Contributor II

Hi Bro,

Got it, thanks for your support.

0 Kudos

798 Views
LPP
NXP Employee
NXP Employee

You are free to use more signal layers as needed beneath top signal and ground layers. You can reproduce NXP reference design by using the same top layer layout, same top substrate material+thickness and top inner plane as RF ground.

Please, take care about thermal design of the PCB. Thicker board will have higher thermal resistance between device and the heat sink.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos