PCA9955B: Is it possible to connect multiple channels to operate multiple LEDs in parallel?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCA9955B: Is it possible to connect multiple channels to operate multiple LEDs in parallel?

跳至解决方案
1,512 次查看
yannick_aeby
Contributor I

We would provide all LEDs with a series resistor. The channels would be interconnected directly at the IC. If we would connect two channels together, we could sink the double amount of current through one track. Is this possible with this IC?

0 项奖励
回复
1 解答
1,454 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yannick,

Yes, it is OK to connect two LED channels together to double LED current in application.

We have had a few customers using such connection in their applications without problems.

Best regards,

Tomas

在原帖中查看解决方案

1 回复
1,455 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yannick,

Yes, it is OK to connect two LED channels together to double LED current in application.

We have had a few customers using such connection in their applications without problems.

Best regards,

Tomas