All:
I am going to state an assumption - please tell me if I am correct.
| Zero | Max | PWM | |
|---|---|---|---|
| LEDn_ON_L | 0x00 | 0x00 | 0x00 |
| LEDn_ON_H | 0x00 | 0x10 | 0x00 |
| LEDn_OFF_L | 0x00 | 0xFF | 0xWM |
| LEDn_OFF_H | 0x10 | 0x0F | 0x0P |
1. If I want zero output, I need to set bit 4 in the LEDn_OFF_H. All other contents of these 4 registers are ignored by PCA chip.
2. If I want max output, I need to set bit 4 in the LEDn_ON_H. Again, all other contents are ignored by PCA chip.
3. A valid PWM is greater than 0 and less than 0xFFF (12-bit max number).
Regards,
Todd Anderson
The PCA9685 datasheet states under heading "7.3.4 ALL_LED_ON and ALL_LED_OFF control" the following: "The LEDn_ON and LEDnOFF counts can vary from 0 to 4095. The LEDn_ON and LEDn_OFF count registers should never be programmed with the same values."
As an experiment, we set LEDn_ON to 0 and LEDn_OFF to 0, and the result was 0 output, the same as setting bit4 of the LEDn_OFF_H register. So, it is almost as if the Full Off bit is not required.
However, to get full on, bit4 of the LEDn_ON_H register does need to be set to get full output. Otherwise, you get 1 cycle of off condition for "FFF".