PCA9626 LQFP48 footprint dimension question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9626 LQFP48 footprint dimension question

910 次查看
therm
Contributor I

In section 19 (page 44) of the PCA9626 data sheet (http://www.nxp.com/documents/data_sheet/PCA9626.pdf​) the footprint drawing recommends dimension D1 to be 0.28mm, and D2 to be 0.5mm (x 8). The drawing would suggest that all 8 outside pads are 0.5mm D2. However, pads this large would not allow adequate solder mask spacing between land. Is there a reason these pads are dimensioned so large? Can the larger pads be ignored and assume D1 for all?

Thanks!

0 项奖励
回复
1 回复

762 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Trevor,

You are right, please use D1 = 0.28mm for all pads.

 

Thanks for pointing this out, I have already asked our application and documentation teams for correction.

Best regards,

Tomas

0 项奖励
回复