PCA9615 - voltage level translator for 1,2V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9615 - voltage level translator for 1,2V

480 Views
matthiasneth
Contributor I

Which voltage level translator can be used in combination with the PCA9615 to connect an I2C device that needs 1,2V as high signal level level and maximum 0.36V as low level  ?

The device will have to recognize the 0.5V low level output of the PCA9615 as low level input.

any recommendations ?

Thank you and Best Regards

0 Kudos
0 Replies