HI,
Is possible to have some information about the output stage of the PCA9615,
information like:
-VOL of the positive and negative output voltage in function of Load,
-Max current output
-Output series resistance.
This is my schematics, for improve the noise rejection i have decreased the pullup resistance to 200 ohm, but the output seems saturated and DP reach a voltage significantly greater than 0V and DM reach a voltage significantly smaller than 5V.
Thanks, Best regards.
HI
All of DSDAP/M,DSCLP/M parameters showing in datasheet page17 Table5,except that there is no others.
Also don't suggest to use 200ohm instead of 600ohm in your circuit!