PCA9614 (Voltage from SDA - GND)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9614 (Voltage from SDA - GND)

875 Views
spanikakamuni
Contributor I

Hello,

I am trying to implement I2c buffer (PCA9614) in one of my applications. I am supplying the buffer from 3V3 source. 

When I measure the voltage between SCL and ground, it measures 3V3. all fine.

but when I measure voltage between SDA and ground, I measure only 0V5. May I know the reason for this behaviour of IC.

0 Kudos
1 Reply

711 Views
darioarias
NXP Employee
NXP Employee

Hello Spanika,

This is not the normal behavior of the device, the default value for the communication lines (SDA and SCL) is Vdd. Do you have the schematic or a picture of your configuration? This will be helpful  to find a possible issue with the connection

Regards,

Darío

0 Kudos