PCA9539 reset issue depending on I²C connection status

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9539 reset issue depending on I²C connection status

45 次查看
JordanSW
Contributor I

Hello,

I am using the PCA9539 I/O expander and have encountered an unexpected reset issue that seems to depend on the I2C connection status.

The issues are as follows:

  • I configure all output ports of the PCA9539 to HIGH via I²C communication.

  • The output pins remain HIGH as expected.

  • However, when I remove the SDA/SCL probes (used for monitoring the I2C bus), the PCA9539 appears to reset — the output pins return to their default state.

  • During this process, VCC remains stable, continuously supplied, and the RESET pin is held HIGH via a pull-up resistor.

  • There is no intentional RESET signal or power cycling from the MCU

Additional notes:

  • This issue does not occur on PCA9538 under identical test conditions.

  • I2C pull-up resistors are present.

  • Power supply is stable and decoupled with capacitors.

  • The RESET pin shows no abnormal activity during the event.

 

I suspect that a glitch or incomplete START/STOP condition when disconnecting the probes might be causing the PCA9539's internal I2C state machine to enter a fault state, which results in a reset-like behavior. However, I have not found any documentation that confirms whether the PCA9539 can clear its output registers without an explicit RESET or power cycle.

As far as I know, in the case of an I2C I/O expander, as long as power is supplied, it should retain its configuration regardless of whether an I2C probe is connected or not. Could you confirm if this understanding is correct?

 

Questions:

  1. Are there any conditions where the PCA9539 may reset its output registers or I2C logic without a RESET pin assertion or power cycle?

  2. Could a glitch on SDA/SCL during probe removal cause the device to enter a fault state and lose its configured outputs?

  3. Why would this behavior occur on PCA9539 but not on PCA9538, given their similar functions?

  4. Is it correct that an I2C I/O expander should maintain its configuration as long as power is supplied, regardless of I²C bus connection?

Any insights or official documentation on this behavior would be greatly appreciated.

Thank you.

 

 

标记 (2)
0 项奖励
回复
0 回复数