PCA85133 Blink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA85133 Blink

362件の閲覧回数
Curly
Contributor II

Hi,

We are using PCA85133 with LCD and want to implement pattern blinking.

Could this LCD driver could achieved blinking specific pattern in display RAM and others could still display without blink?

First, set blinking mode with normal blinking and blink frequency selection is 3 then send display RAM through load-data-pointer. The patterns will blink as I expected, but if other display RAM was enabled, the whole pattern will blinking as well.

 

Thanks.

タグ(1)
0 件の賞賛
1 返信

346件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Curly,

I hope all is great with you.

PCA85133 supports two kinds of blinking methods which are whole display blinking and an arbitrary selection of LCD segments to blink, please see below section 7.11 Blinking in the datasheet for the detail explanations for blinking methods.

diazmarin09_1-1661180865780.png

 

I hope this information helps.

Regards,

David

0 件の賞賛