PCA85133 Blink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA85133 Blink

368 Views
Curly
Contributor II

Hi,

We are using PCA85133 with LCD and want to implement pattern blinking.

Could this LCD driver could achieved blinking specific pattern in display RAM and others could still display without blink?

First, set blinking mode with normal blinking and blink frequency selection is 3 then send display RAM through load-data-pointer. The patterns will blink as I expected, but if other display RAM was enabled, the whole pattern will blinking as well.

 

Thanks.

Tags (1)
0 Kudos
1 Reply

352 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Curly,

I hope all is great with you.

PCA85133 supports two kinds of blinking methods which are whole display blinking and an arbitrary selection of LCD segments to blink, please see below section 7.11 Blinking in the datasheet for the detail explanations for blinking methods.

diazmarin09_1-1661180865780.png

 

I hope this information helps.

Regards,

David

0 Kudos