PCA85063A with external oscillator?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA85063A with external oscillator?

Jump to solution
837 Views
theo1
Contributor I

Can you use a PCA85063A RTC with an external oscillator?

Thanks.

0 Kudos
1 Solution
692 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Yes, you can use an TCXO instead of a crystal. In this case no crystal will be connected to the OSCI and OSCO pins. Instead, the external oscillator is connected to the OSCI pin while the OSCO pin must be left floating.

 

Regards,

Jose

View solution in original post

3 Replies
692 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

The PCA85063A RTC does not include internal oscillator, only PCF2127 and PCF2129 from the NXP portfolio include internal oscillator, so, the PCA85063A RTC circuit requires one external tuning fork quartz as resonator (external oscillator) to work.

What it is integrated in the PCA85063A are the oscillation capacitors and therefore there is no need for external capacitors.

The quartz crystal must be placed close to the RTC circuit, avoiding long lines which may pick up noise.

Regards,

Jose

0 Kudos
692 Views
theo1
Contributor I

Thanks Jose.

What I mean is can you use an TCXO with a logic level output instead of a crystal?

0 Kudos
693 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Yes, you can use an TCXO instead of a crystal. In this case no crystal will be connected to the OSCI and OSCO pins. Instead, the external oscillator is connected to the OSCI pin while the OSCO pin must be left floating.

 

Regards,

Jose