PCA2129 problem in OSF value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA2129 problem in OSF value

1,064 Views
mouaiadsalaas
Contributor I

hello .

I have a problem when i read seconds register of PCA2129 the osf bit is always 1 so that make my recieved data are not right so can you please tell me how to set that bit 0 ?? or what should i do to solve this problem so osf would not be 1 

I am using SPI protocol in TMS570LS07 mcu with PCA2129 and I am sending TX_DATA[0]=0xA3;to read seconds register 

 

uint16_t TX_DATA[100];
uint16_t RX_DATA[100];


uint8_t readsecondsRegister() {
gioSetBit(spiPORT1, 0U, 0);
TX_DATA[0]=0xA3;
spiTransmitData(spiREG1, &dataconfig1_t, 1, (uint16_t*)&TX_DATA[0]);
spiReceiveData(spiREG1, &dataconfig1_t, 1, (uint16_t*)&RX_DATA[0]);
gioSetBit(spiPORT1, 0U, 1);
return (uint8_t)RX_DATA[0];
}

 

Tags (3)
0 Kudos
Reply
0 Replies