PCA 21125 Xtal load capacitor impact to RTC accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA 21125 Xtal load capacitor impact to RTC accuracy

269 Views
GregB_in_Michigan
Contributor I

For PCA 21125 RTC...

Data Sheet says "The frequency tolerance depends on the quartz crystal tolerance, the
capacitor tolerance and the device-to-device tolerance (on average 5  106). An
average deviation of 5 minutes per year can easily be achieved."

If Xtal load capacitance goes up or down 10pF, what is the impact to RTC accuracy?

Clock speed Hz goes up or down if capacitance varies +10pF?   Varation impact or measurement difference between 32768Hz and 32778Hz is not easy to differentiate with typical lab equipment.

gbober@lgensol.com

0 Kudos
5 Replies

236 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

For your question:

If Xtal load capacitance goes up or down 10pF, what is the impact to RTC accuracy?

[gw]without the suitable CL matching, the clock also has the accuracy issue.

0 Kudos

230 Views
GregB_in_Michigan
Contributor I

For many years we had 10pf 5% Xtal load cap with the crystal.   Then it was recommended to

change to 18pF 5% tol.    What would have been the normal RTC time counting impact of such a change?

Is there an equation to help me determine how the 8pf shift and +/-5% variation impacts the RTC time accuracy?

0 Kudos

193 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

You can use below equation to calculate the Cext value to match crystal requirement CL value, whatever it's 18pF or 10pf

guoweisun_0-1713783622710.png

 

 

 

 

guoweisun_0-1713774633190.png

 

0 Kudos

185 Views
GregB_in_Michigan
Contributor I

thanks... but for PCA21125 what is delta_Frequency/delta_Cload sensitivity?  no sensitivity identified in Tables 41 to 43 of component specification.   The Cload equation is from Table 42.  Section 14.2 only mentions adjusting the pin load capacitance as a method to improve accuracy... thus there is an impact to accuracy...the +/-Hz or seconds over a span of time impact is not stated.

 

 

0 Kudos

158 Views
guoweisun
NXP TechSupport
NXP TechSupport

---

Section 14.2 only mentions adjusting the pin load capacitance as a method to improve accuracy... thus there is an impact to accuracy...the +/-Hz or seconds over a span of time impact is not stated.

---

I comprehend that the error between calculated CL and actual CL requirement will impact the RTC accuracy.

0 Kudos