Hi.
I have some questions about P82B96_TSSOP.
The top part is marked 82B96. Numbers such as '01 01 028' are written below.
1. Could you tell me about the meaning of the numbers below?
I have two different numbers.(01 01 028, 01 02 030)
2. If the meaning of the number is different, is the resistance value of p82b96 different?
When the buffer was replaced, the resistance value of the power input pin changed.
Have a good day.
Thanks.