P3S0200可以工作在1.8V的IIC上吗

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3S0200可以工作在1.8V的IIC上吗

249 Views
赵中飞
Contributor I

P3S0200的VCC我用3.3V,IIC我用1.8V可以吗

0 Kudos
Reply
1 Reply

240 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Zhao,

please refer to the Table 7. in the P3S0200 datasheet. The VCC voltage sets the VIH and VIL levels for the input pins. If VCC=3.3V, than minimum voltage required on the input pins, to be recognized as logic high it 0.46*VCC=0.46*3.3V=1.518V. You can use the 1.8V for the input pins. The 1.8V will be recognized as logic high.

JozefKozon_0-1700481975929.png

 

With Best Regards,

Jozef

0 Kudos
Reply