Thanks a lot for your valuable comments.
There was actually a conflict with the LAW settings and address range defined in OR and BR registers.
For testing purpose,we are only configuring the chip select connected to CPLD that is CS3 , Following are the new configuration settings:-
1. Two LAWs are being assigned to local bus interface
LAW1 : E8000000 - F8000000
LAW2 : FFDF0000 - FFE00000
2. BR3: FFDF8000
OR3: FFE00000
But still there is no success, CS3 is not asserted when we try to access any location within the specified range.
Kindly guide about the possible causes for the same.