Hello,
I have a OM2NTP5332 NTAG 5 board and I want to use it with a raspberry PI. I want to establish a communication between the raspberry's i2c bus and the board.
I read the board's manual, but I don't find how to use it on a raspberry with Raspberry PI OS (debian based). I had tried to find some python smbus code example for using the board on the web, but I found nothing.
Can someone help me ?
Thank you in advance.
Hello sir, thank you for your preference for using our products.
Unfortunately, we don't have any example of the NTAG 5 connected to the Raspberry Pi. Do you happen to have any first attempts that you could share with us? Especially if you have a log that we can start working with.
Hello,
thank you for your answer. I connect the board to the raspberry PI GPIO by the SCL and SDA connector on the board to the GPIO on the raspberry GPIO2 (SDA) and GPIO3 (SCL) and I powered the board with on a 5V pin. On Raspian the board his recognized on the I2C port when I use the i2cdetect command on the shell. I try to communicate with the board by scanning all the register with the i2cdump command, all of them have the 0xFF value. When I try to write another value with the i2cwrite command on one of the register the command return no error but the register value is not changed. I tried the libnfc library (GitHub - nfc-tools/libnfc: Platform independent Near Field Communication (NFC) library), but she returns errors with the board and no official pilot for the board is available. I also tried to use this software like is describe on your website Easy set-up of NFC on Raspberry Pi - NXP Community. I modified the GPIO configuration in the phTmlNfc_alt.h file, to adapt to my configuration like to describe in this documentation AN11697 (nxp.com) but it did not work. Finally, I tried to use the python smbus library to communicate with the board, but I failed to find in which register I have to read to have access to the data on the tag I put on the board.
Hello,
Is the board only made to run on an i2c to USB bridge with the cockpit application or it can be used with other hardware like a Raspberry or an Arduino for example ?
Thank you in advance