No Processor Expert tool for SKEAZ64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Processor Expert tool for SKEAZ64

579 Views
547416104
Contributor III

Hello every one,

    I used S32DS IDE to create SKEAZ64 application project, and select KEAZ128 SDK, after the project is created, I can not see Processor Expert tool, whether the skeaz64 is not supported by Processor Expert? thanks!

 

 

0 Kudos
1 Reply

545 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

KEA SDK does not support Processor Expert, so you can not see it.
Please refer the examples in FRDM-KEAZ Freedom Evaluation Board – QSP(FRDM-KEA-QSP\Quick Start Package v8\Code Project Examples and Sample Drivers (Evaluation Grade Only)\FRDM-KEAZ64\Driver Test SW for KEAZ64\Driver Test SW for KEAZ64)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos