Does anyone have an S-Parameter file available for the MRFE6VS25GNR1 or MRFE6VS25NR1 that covers 30 MHz to 100 MHz? The S-Parameter file on the NXP web site starts up at 200 MHz. I would like to do some preliminary analysis from 30 to 100 MHz using S-parameters but they aren't available. Also, I can't use the ADS model at this time since I don't presently have ADS. I attached the .s2p file that is available on the NXP site but it's not sufficient for my needs. Thank you.
I have the same issue. I, too, need the S-parameter values below 200MHz. I am curious why these are not supplied. This is an issue for multiple parts which are specified for low frequencies, but without the S-Parameters supplied for frequencies below 150MHz or 200MHz.