Need MRFE6VS25 S-parameters that cover 30 to 100 MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need MRFE6VS25 S-parameters that cover 30 to 100 MHz

1,781件の閲覧回数
eric_hooker
Contributor I

Does anyone have an S-Parameter file available for the MRFE6VS25GNR1 or MRFE6VS25NR1 that covers 30 MHz to 100 MHz?  The S-Parameter file on the NXP web site starts up at 200 MHz.  I would like to do some preliminary analysis from 30 to 100 MHz using S-parameters but they aren't available.  Also, I can't use the ADS model at this time since I don't presently have ADS.  I attached the .s2p file that is available on the NXP site but it's not sufficient for my needs.  Thank you. 

0 件の賞賛
返信
6 返答(返信)

1,503件の閲覧回数
Stephan_Orzada
Contributor I

I have the same issue. I, too, need the S-parameter values below 200MHz. I am curious why these are not supplied. This is an issue for multiple parts which are specified for low frequencies, but without the S-Parameters supplied for frequencies below 150MHz or 200MHz.

0 件の賞賛
返信

910件の閲覧回数
MFrank
Contributor I
Hey. Did you get the S2p parameters from 30 MHz for this transistor?
0 件の賞賛
返信

899件の閲覧回数
Stephan_Orzada
Contributor I

Unfortunately not. I did not even get a reply of any sort.

0 件の賞賛
返信

887件の閲覧回数
MFrank
Contributor I
Too bad. Because I'm currently designing an amplifier in this band pass. Did you succeed with this amplifier?
0 件の賞賛
返信

883件の閲覧回数
Stephan_Orzada
Contributor I

From the S-Parameters at 200, 300 and 400 MHz I estimated the following model:

Linear_Model_MRFE6VS25N_S_Orzada.jpg

This worked quite nicely for me. This part is now a driver stage in a 2 kW_peak MRI-Amplifier. For the real amplifier I was able to use exactly the values  for the matching network I obtained from the spice simulations at 128 MHz.

0 件の賞賛
返信

861件の閲覧回数
MFrank
Contributor I
Thank you for the information.
Regards
0 件の賞賛
返信