NX5P3290UKZ EN , FO & CAP pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NX5P3290UKZ EN , FO & CAP pin

864 次查看
TST_S
Contributor I

Dear Sir/Madam,

I would like know whether both EN & FO pin can be left floating for logic 'Low‘ condition ?

or both pins need pull down resistor to make it 'Low' ?

Can help to explain in detail why the CAP pin capacitor value have to be 1nF ?

Thanks.

0 项奖励
回复
3 回复数

858 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Tan,

both EN and FO pins have internal 1MOhm pull down resistors, so if you will leave them floating, both will be pulled down.

JozefKozon_0-1658144139939.png

The Cb=1nF capacitor on the CAP pin is a recommended value. The capacitor is used to fast recovery of the MOSFET. 

JozefKozon_1-1658144413038.png

JozefKozon_2-1658144947804.png

With Best Regards,

Jozef

0 项奖励
回复

855 次查看
TST_S
Contributor I

hi Jozef,

Thank you for your reply.

1M ohm is quite big for pull down, can I use external 0 ohm to pull down to always turn off the

feature of FO pin ?

Best regard

 

0 项奖励
回复

849 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Tan,

yes, you can connect the FO pin directly to the GND if you don't want to use the Fast Turn On feature.

With Best Regards,

Jozef

0 项奖励
回复