NX5P3290UKZ EN , FO & CAP pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NX5P3290UKZ EN , FO & CAP pin

852 Views
TST_S
Contributor I

Dear Sir/Madam,

I would like know whether both EN & FO pin can be left floating for logic 'Low‘ condition ?

or both pins need pull down resistor to make it 'Low' ?

Can help to explain in detail why the CAP pin capacitor value have to be 1nF ?

Thanks.

0 Kudos
Reply
3 Replies

846 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Tan,

both EN and FO pins have internal 1MOhm pull down resistors, so if you will leave them floating, both will be pulled down.

JozefKozon_0-1658144139939.png

The Cb=1nF capacitor on the CAP pin is a recommended value. The capacitor is used to fast recovery of the MOSFET. 

JozefKozon_1-1658144413038.png

JozefKozon_2-1658144947804.png

With Best Regards,

Jozef

0 Kudos
Reply

843 Views
TST_S
Contributor I

hi Jozef,

Thank you for your reply.

1M ohm is quite big for pull down, can I use external 0 ohm to pull down to always turn off the

feature of FO pin ?

Best regard

 

0 Kudos
Reply

837 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Tan,

yes, you can connect the FO pin directly to the GND if you don't want to use the Fast Turn On feature.

With Best Regards,

Jozef

0 Kudos
Reply