Dear Sir/Madam,
I would like know whether both EN & FO pin can be left floating for logic 'Low‘ condition ?
or both pins need pull down resistor to make it 'Low' ?
Can help to explain in detail why the CAP pin capacitor value have to be 1nF ?
Thanks.
Dear Tan,
both EN and FO pins have internal 1MOhm pull down resistors, so if you will leave them floating, both will be pulled down.
The Cb=1nF capacitor on the CAP pin is a recommended value. The capacitor is used to fast recovery of the MOSFET.
With Best Regards,
Jozef
hi Jozef,
Thank you for your reply.
1M ohm is quite big for pull down, can I use external 0 ohm to pull down to always turn off the
feature of FO pin ?
Best regard
Hi Tan,
yes, you can connect the FO pin directly to the GND if you don't want to use the Fast Turn On feature.
With Best Regards,
Jozef